Other Parts Discussed in Thread: TLK106, TLK105
Hello,
we have got a Texas Instruments Evaluation (EVM) Kit [TLK106CUSEVM] and tried to connect that board with one of our products instead of our standard PHY [micrel_KSZ8031RNL].
We are currently using the RMI Interface and modified the board according to the following steps:
|
Modification of the TLK 106 PCB for usage with the RMII |
||
|
Change J1 to PD (RMII) |
|
✓ |
|
Connect J10 (RMII PU) |
|
✓ |
|
Disconnect R71 and R72 |
|
✓ |
|
Populate R73 (0Ohm) |
|
✓ |
|
Remove XTAL1 |
|
✓ |
|
Populate a 50MHZ oscillator at U5 |
✓ |
|
Problem:
There is no data transmission via Ethernet between test device and PC.
We can’t even ping to the device.
Solution approaches:
We connected two of our Controllers, one with the usually used PHY and one with the TLK106.
According to the terminal output of the standard controller the Ethernet Signal is interrupted a long time which causes the connection to disconnect continuously.
I also used a logic analyzer to record the MDIO signal. There is one significant difference between the signal of the usually used PHY and the TLK 106. The PHY Adress and the Register Adress are identical but the Register Data differs in two bits.
What information do these two bits contain?
Usually used PHY:
TLK 106:
Do we need to do any software changes?
Is there any possibility to get the TLK 106 to work with our device?
Best Regards
Daniel