Other Parts Discussed in Thread: DS30BA101, LMH0303, DS15BA101
Hello, I need to implement a bidirectional LVDS to pass a 1pps signal with 500ps timing accuracy. I am considering using a pair of DS30BA101 devices to do this. (Note I tried using typical MLVDS buffers, but their device propagation delays are too large). The problem I'm facing with the DS30BA101 is that its outputs cannot be tri-stated. So, to solve this problem, I am considering using a logic-controlled power switch to shutoff the buffer which won't be used for a given direction flow. In order for this to work, I need the output stage of the driver to go into high-impedance when the power is shut off. Does anyone know if the DS30BA101 output stage goes into high Z (10K or higher) when the power is shut off?
Thanks, Gary A.