This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1540, ISO1541



1. VCC1 and VCC2>2.8V, THE OUTPUT SHOULD BE "H" FOLLOWING INPUT "H". THE TABLE SHOW "Z", IT SHOULD BE TYPO ? IT WOULD CONFUSE THE ENGINEERS MISSING "H" OUTPUT.