Other Parts Discussed in Thread: TPD6E001
Hi,there
i am designing a USB based project.i choose the TPD6E001 as the ESD protection device,i have two questions that need your help. i've uploaded the USB part of my schematic for illustration.
1.As indicated,two ground symbols,the usb shield ground and the signal ground,exist in the system,so which of
the two grounds should the common ground of ESD device be connected to?i connect to the signal ground,but i'am
not sure whether it will work.
2.i google on how to bridge shield ground and signal ground and two different solutions are found:
(1)Place a large resistor(usually 1M ohm) paralleled with a capacitor between the two grounds.
(2)Isolate the two grounds with a 0ohm resistor or a ferrite bead.
Can someone explain the two solutions in detail, in which situation they are applicable?
Thanks for your attention!
Sincerely,