This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS34RT5110 – About the available input signals

Guru 21045 points

Other Parts Discussed in Thread: DS34RT5110

Hi Team,

 

My customer would like to use DS34RT5110 with the “1080p120Hz” and “4k2k30Hz” input signals.

If about 3Gbps per data channel, is the each input signal supported by DS34RT5110?

And, please let me know, if you have the information that DS34RT5110 has been used successfully with this input signals.

 

Regards,

Kanemaru

  • Hi Kanemaru,

    DS34RT5110 is capable to support 3.4Gb/s per data lane as an equalizer.

    I do not recommend DS34RT5110 as a 3.4Gb/s retimer, when the input video source contains high amount of lower frequency jitter (< 4MHz).

     

    regards,

    TK Chin

     

  • Hi TK-san,

     

    Thank you for the information.

    I understood that DS34RT5110 as an equalizer (Bypass pin = High) is available with the “1080p120Hz” and “4k2k30Hz” signals.

    Is my understanding correct?

     

    If you contact to below my e-mail address or let me know your e-mail address,

    I can send the customer information.

    I’m looking forward to hearing from you.

     

    [my e-mail address]

    Kanemaru-h@clv.macnica.co.jp

     

    Regards,

    Kanemaru

  • Kanemaru-San,

    Your understanding is correct. If you pull Bypass pin high it bypasses the retimer and enables the device to act like an equalizer only. With Bypass pin high, you can use the EQ0, EQ1, & EQ2 pins to set the equalizer gain response. Also, you can use DE0 and DE1 to set the de-emphasis as needed. Please note DS34RT5110 is rated up to 3.4Gbps

    Regards,,,nasser

  • Hi Nasser-san,

     

    Thank you for your prompt reply.

     

    ------------------

    [Q1]

    I understood that DS34RT5110 can allow passage of the each signals,if about 3Gbs per data channel.

    --------

     

    [Q2]

    I believe that we can’t use de-emphasis function, when Bypass pin = high.

    Is my understanding correct?

     

    My customer would like to use DS34RT5110 with A-side cable =3.5m.

    Please let me know if you have any advice.

    --------

     

    [Q3 (additional question)]

    Must we not change the loop filter components(2.2nF and 3.3kohm) ?

    So, is this components recommended at all condition?

     

    ------------------

     Regards,

    Kanemaru

  • Hi Nasser-san,

     

    I apologize. I have one more question.

     

    [Q4]

    Do you have a data that DS34RT5110 allowed passage of the signal(“1080p120Hz and “4k2k30Hz””).

    My customer would like to confirm that the each signal is supported by DS34RT5110.

     

    If you don’t have a data, could you please measure that?

    We would appreciate it if you could evaluate this.

     

    Regards,

    Kanemaru

  • Hello expert,

    Can you kindlky advise Kanemaru-san's inquiry? Customer is still asking us frequently.

    Thank you for your suppor in advace.

    Best regards,

    Daisuke KAWASAKI

  • Hi Mita-san

     

    Thank you for the information.

    Iunderstood. thank you very much.

     

    Regards,

    Kanemaru