This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Parallel bus level translator with hysteresis



Hi, please help with product selection. I have unidirectional cmos transmit (4) and receive (12) signals at the end of a long parallel bus. I need 5v to 3v3 level translation with hysteresis for reception, and 3v3 to 5v driver to transmission.

Can you suggest a suitable level translator family that includes hysteresis?

  • Hi Anthony,

    To make sure I understand your question correctly. You have 16 single-ended channels that you would like to level shift (12 in one direction and 4 in the other). These are not differential signals or signals that need to be isolated, correct?

    Thanks,

    John