This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using HDMI or DisplayPort to show image data on a 4.3" display

Hi.

I've been asked about an interface problem. The display data are sending from a 3th party module via DisplayPort or HDMI/DVI. The planned display is 4.3" large but only capable to work with 12 MHz resolution.

Is there a way to convert DP, DVI or HDMI to 8 to 12 Bit RGB parallel data?

Thanks for your help!