This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK3134 Cable Length

Hello,

I am trying to find drivers for the following interfaces that can drive cables over 3m:

XAUI interface at 3.125 Gbps

LVDS at 160 Mbps

I found the TLK3134 that can work with XAUI, and has built in de-emphasis, and there a few options for LVDS. I cannot find information on cable lengths that these can drive, though. 

Thoughts?

Thanks,

Michael 

  • Michael,

     

    What type of cable is the customer wanting to drive as what data rate 3.125Gbps? 

    We did a study a while back on driving 600mbps over Cat5 cable.  But at 3.125Gbps, the customer will need to use higher quality cable such as twin-ax.  With twin-ax and proper setup you, transmission  distance up to 10m can be achieved but it all depends on the loss of the cable.

    -Atul