Other Parts Discussed in Thread: TPD12S016, TPD12S520
Hi,
Can I use TPD12S016 for ESD protection and level translation (3.3->5V) for HDMI Input?
From the datasheet, i feel it is fine for TMDS, SCL, SDA and CEC lines (they are bidirectional). But regarding, HPD line, it is unidirectional and the input of HPD is 5V level, while output is 3.3V level. However, in case of HDMI input, we need input at 3.3V at output at 5V.
Can you please confirm on the above point? Also, if above iC is not suitable, can you please suggest an alternate IC?