Other Parts Discussed in Thread: SN65LVDS822
I would like to use the SN65LVDS822 to interface LVDS signal to an LCD panel with 24-bit TTL. I understand that the outputs on the SN65LVDS822 are CMOS. It looks like the voltage levels for the high and low match, but is there a compatible IC that is true TTL output? or is there anything external I can do to get better results.
Aside from the CMOS issue, the IC is a perfect match for the application. I got the LCD to function correctly, but clock on the output looks more like a sine wave.