Other Parts Discussed in Thread: TUSB1310
Hello everyone,
I met a problem when I try to use TUSB1310 on my Xillinx FPGA.
According to the datasheet, the output ULPI_CLK should be 60MHz.
I input a 40MHz xstal clock on pin "XI", and I set the ULPI_DATA[5:4] to 2'b11 when PHY_RESETN and RESETN are
de-assertion.
But it looks like no matter which value I set to ULPI_DATA[5:4] when I reset TUSB1310, the output ULPI_CLK always
is 120 MHz.(I have try 2'b00 and 2'b11)
Seems like it didn't catch my strap setting.
Any suggestion for me?
Thank you
Chiayu Lu