Other Parts Discussed in Thread: TFP410, TFP401
Hello, I'm having some troubles with a TFP410. See the attached circuit; basically an HDMI input signal is received by a TFP401, then sent either to a video DAC to generate a VGA signal and to a TFP410 to generate an HDMI signal. The VGA signal is generated correctly (so the TFP401/DAC section should be ok), but nothing comes out from the TFP410. All signals seem to be fixed, pulled up to 3.3V by the sink (a common monitor).
I've already tried several things: decoupled the HDMI outputs, changed the clock polarity, and switched to low-swing mode by setting Vref=0.9V (the input signals are a little attenuated, they swing up to 2.3-2.4V - this could be related to the fact that the signals are "split" between two devices, or it could just be the oscilloscope's fault). Now I'm going to try to fiddle with the deskew control, but I don't think it will work, everything seems quite dead and I hope I've just made some silly mistake.
Thanks!
(update) I correct myself: only the TMDS_CLK+ and CLK- are pulled to 3.3V. The other six signals (D0+, D0-, D1+, D1-, D2+, D2-) are all fixed around 0.2-0.3 V. I don't know if there is any high-speed signal in there, with my lousy 200 MHz, 2 GSPS oscilloscope I can't see anything. Also, MSEN works correctly.
(update 2) Now I'm quite sure that the TFP410 doesn't generate any signal, it's not my oscilloscope's fault. I've measured another HDMI signal with it and I can see some clear activity (thanks to the undersampling). Therefore what I'm seeing on the TFP410 outputs should be the "real deal": a 3.3 DC voltage on TXC+ and TXC-, and a 0.3 DC voltage on all the other outputs. I've also checked again the CMOS signal levels and they are actually ok, the signals change very cleanly on the clock falling edge without any evident skew, so everything looks ok from the CMOS side. I'm starting to believe that TFP410 doesn't like what the TFP401 is generating, but I find this difficult to believe: they look like they are made to work back to back!