Other Parts Discussed in Thread: TFP401A-EP, DS16EV5110
I have a TFP401A-EP whose inputs are driven by an equalizer DS16EV5110.
No DVI source is connected to the equalizer. Both lines of its output clock pair are idle at 3V (goes up to 3.3V is the EQ is powered down).
So far that looks ok for me.
Meanwhile, the TFP401A-EP outputs chaotic signals (3.3Vpp noise) on all data lines while the output clock (ODCK) line outputs some kind of 300MHz sine wave full of jitter and with some glitches on the peaks.
DE output tries to go down from time to time but so briefly that it does not even reach GND.
My scope has 1GHz BW and I am properly probing with a GND spring. It is unlikely to be a measuring issue.
It also heats a lot. My estimation is around 600mW power consumption for the TFP401A-EP and the EQ together.
That does not look good to me.
Is that an expected behavior?
Regards,
Fred