Other Parts Discussed in Thread: TUSB7320, TUSB7340
1) TUSB7320 PCIE_RX polarity
Can a customer invert the polirity of PCIE_RX?
Can PCIE_RXP and PCIE_RXN be swapped?
2) TUSB7320 PCIE_REFCLK
Can a customer invert the polirity of PCIE_REFCLK?
Can PCIE_REFCLKP and PCIE_REFCLKN be swapped?
3) If 2) is yes, is there a description or a definition about the PCIE_REFCLK polarity inversion in PCI Express Specification? For example, PCIE_REFCLK must automatically detect the inversion, register settings are needed to swap the polarity and so on.