This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB913A

Please advise me on choosing connecter and cable used with DS90UB913A/914A

DS90UB913EVK and DS90UB913A EVK are using Rosenberger’s connector and
FAKRA connecter respectively.
They also use STP and Coaxial cable respectively.

Are there any criterion on the specifications bellows.

1. Return loss must better than xx dB between yy and zz MHz.
2. Insertion loss should be smaller than xx dB between yy and zz MHz.
and loss curve should be well coincide to 1/Sqroot f curve with in xx dB tolerance.
3. Impedance of the connecter (or cable) must be 50 ohm +/-xx % (or 100 ohm diff +/- xx %)

If there are any other parameters to be counted on, please device me too.

Mita