Other Parts Discussed in Thread: ISO7241C
What is the typical supply current of the ISO7241C when both enable lines are low, Vcc1 is at 0V, and Vcc2 line is connected to a 5V supply?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO7241C
What is the typical supply current of the ISO7241C when both enable lines are low, Vcc1 is at 0V, and Vcc2 line is connected to a 5V supply?
Hi David,
Since the internal oscillator remains on and the outputs are just placed in a high impedance state, the current draw remains almost identical to when the EN signal is pulled high.
I just went into the lab to verify this, and the device I tested drew 12.65mA of current with the EN pin tied high (5.0 volts), and 12.62mA with the EN pin tied to GND2.
Please let me know if you have any other questions,
John
Thank you, that confirms what I'm seeing on my end. I appreciate the fast response.