Other Parts Discussed in Thread: LMH0394, LMH0387
What is the proper method of attaching a balun or transformer to the front end of the lower power LMH0394(2.5V) or similar. Input for this part is showing (typically) that it is capacitive coupled, likely do to a bias imposed by the LMH0394.. I have two areas of interest with the magnetics.. Balun specific to a customer request, and transformer for isolation of ground loops.. Balun at the SDI 1.25v offset 800mv swing level, transformer likely both the SDI and LVDS/CML levels, prior to the input of a reclocker such as the LMH0366 or LMH0346
-D