Hello,
I have a question regarding the use of 33 ohm resistors as recommended in SLVA531A paragraph 4.3. If the PHY is placed close to the MAC device (in my case an FPGA) are these series resistors still necessary? What is the value (33 ohm) based on? Should the PWB traces be 33 ohms as well if the series resistors are used?
Thanks for any help you can give.