This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPD12S520DBTR Differencial interface



Hi,

I am using TPD12S520DBTR device in my project. I have found pin 4 and 35 are same. Is it that I have to short these pins in the schematic.  Please clarify as soon as possible.

Thanks and Regards,

Sankar.K

  •  Sankar,

    That's correct. Each differential line has two pins, which should be electrically connected in the schematic and on PCB. Here they are listed:

    Pins to short together
    Pin Name Pin Number
    TMDS_D2+  4, 35 
    TMDS_D2–  6, 33 
    TMDS_D1+  7, 32 
    TMDS_D1–  9, 30 
    TMDS_D0+  10, 29 
    TMDS_D0–  12, 27 
    TMDS_CK+  13, 26 
    TMDS_CK–  15, 24 

    Regards,