Other Parts Discussed in Thread: ISO3080
I would like to use the ISo3080 as an alternative for the ADM3080.
The apear to be almost the same function,
The main functional important difference I see is pin 7 and pin 10 on the ISO3080 are also gnd and for the ADM2491 those are NC but must be left floating.
For the TI part pin 7 and 8 are labeled GND1 as are pin 9 and pin10 for GND2
Now the main point is Must pin 7 and pin 10 be used for gnd or could these two pins be floating because they are already internally connected and only pin 8 and pin 9 connected is also good.
The gnd pins at 2 and 11 are the same for both parts.
Thaks,
Bert