Other Parts Discussed in Thread: HD3SS6126EVM, HD3SS6126
Hi, I am designing USB3.0/2.0 device with HD3ss6126. When I read the HD3SS6126EVM schematic download from TI.com today, I found U1(HD3SS612x Mux switch) has different pins with HD3SS6126 datasheet.
Pin 1, 2,35, 36, 37,38 42 are NC from HD3SS6126 datasheet, but not in the HD3SS6126EVM schematic. Apparently there are some errors, but which should I trust?
Another question is: from HD3S6126 datasheet, max voltage range on differential I/O (SSA, SSB, SSC, supply voltage) is 4V, but from HD3SS6126EVM schematic, USB connectors (U2, U21) are directly connected to pins of HD3S6126. As far as I know, the voltage on differential signal pins of USB host is 5V, will it burn this chip?
So confusing about this chip and Evaluation board. Please help.
Thank you.