Other Parts Discussed in Thread: DS80PCI402
HI have a new design with a DS80PCI402 buffering 4 lanes. I have the device set up in loopback mode with an FPGA sending test data through the high speed interface. I have it set up in SMBUS/I2C mode (ENSMB 1K pull-up). I have tried many register writes and I can read back the data from the device just fine. However, I see no changes in the device operation. I have enabled all the pin overrides and tried to power down all channels, change the loopback to kill the communication interface, force all chanels to electrical idle, and changed the equalizer settings from 00 to FF and I see no change in bit error rate or link status. Why isn't the device committing changes written to the registers?