Other Parts Discussed in Thread: TLK106L, DP83640
Dear Sir
I have some question about TLK106L
1.Fast Link Down Modes :
What's this feature benefit ? Is it mean if I meet some problem just like signal or energy loss ,TLK106L could Drop link from 100Mbps to 10Mbps within 10uS?
2.IEEE1588 SFD :
SFD seems like need to work with processor or controller ,Is it mean If this controller doesn't support IEEE1588 function
I need to change to use DP83640 than I will have IEEE1588 function?
How about the Sync timing of TLK106L? I refer to DP83640 can be under 10ns
Thanks