Other Parts Discussed in Thread: DS90LV012A
I am new to LVDS technology so please correct me if I am wrong. I have a board that has LVDS driver with 100ohm resistor termination. I am trying to provide the output differential signal from the driver to a LVDS receiver(DS90LV012A 3V LVDS Single CMOS Differential Line Receiver). As per the datasheet the output of the LVDS receiver should be a TTL signal. So in order to test the IC I passed 100 mV sine wave to IN+ pin of the IC and grounded the IN- pin. So theoretically shouldn't I be getting a TTL signal of the same voltage as the sine wave?