Other Parts Discussed in Thread: SN75115
I just wanted to confirm that to use the SN75114N as a differential push-pull driver that I would tie together YP and YS as well as ZP and ZS and then use Y (the combined YP-YS) and Z (the combined ZP-ZS) as my differential push-pull pair. I am about 99%, but would like to get to 100%. :)
I was not able to find an app note with a diagram for this mode. The datasheet does indicate in the first bullet item that there is a "choice of ... totem-pole outputs."
Here is a link to the 75114 datasheet:
http://www.ti.com/lit/ds/symlink/sn75115.pdf
Thanks!