This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Configuration of DSI to eDP bridge SN65DSI86 2048x2732

I would like to configure the SN65DSI86 DSI to eDP bridge chip to drive a ES Panel, resolution 2048x2732.

First, I configure the SN65DSI86 to Color Bar Generator(RGB).

this picture is pannel(2048x2732) which drive color bar generator(RGB) in the SN65DSI86.

Marked 'X' is right color and Marked 'O' is wrong color.

in other resolution,   the SN65DSI86 display the all embedded  pattern.

ex) 1600x2560 , 1800x3200   etc....

If this does not display the color bar pattern, can't drive the panel using the DSI port?