Other Parts Discussed in Thread: TLK2711EVM-CVAL
USED TLK2711A EVM(TLK2711EVM-CVAL ). Clock sources is XC3S700AN.Voltage Set LVCMOS25.
Using Jumper to set it constant. The EVM board transmit word "B5B5-B5B5";(Hex)
Using SMA cable to connect DIN-DON,DIP-DOP.(Serdes Port conneted)
The Logic analyzer capture its rxd.Trigger signal is rxclk.
In scope.I find B7B7-B7B7.(Sometime it is 4B4B-4B4B or 4A4A-4A4A)
TLSB and TMSB used jumper to pulldown.
Q1:tlk2711a can not support signal to confirm PLL locked. Master device wait 100us after Power ON. IS it the only one way to confirm PLL locked ?
Q2:Clk keep transmit ,after Power ON.200us later, Enable signal set valid.I found some EVENT in RLSB&RMSB.When i can implement tlk2711,I need to wait ? How did i confirm tlk2711 ready?
Q3:The EVM power on.Enable pullup.Keep transmitting clk.TLSB&TMSB pulldown.RXCLK can work?
Q4:When I pullup TLSB/TMSB, I Can see K code in RXD7-RXD0/RXD15-RXD8?( Using SMA cable to connect DataIn_N-DataOut_N,DataIn_P-DataOut_P)
Thanks for your attention.