Other Parts Discussed in Thread: TUSB1310A
Hi I'm looking at the TUSB1310A datasheet (http://www.ti.com/lit/ds/sllse32e/sllse32e.pdf) and have a few questions on the setup for this chip.
VBUS resistors
1) On p27 Section 5.1 It shows the VBUS pin of the TUSB chip connected to the voltage divider of the 90.9K and 10K resistors. Is it correct that the power rating on the 90.9K resistors should be 5+ Watts because USB3.0 specifications say that VBUS is 5V and can carry 900mA of current. Since most of the voltage drop would be across the 90.9K resistor (5V * 90.9/(10+90.9) ), the power rating seems like it should be 5+ watts.
2) If #1 is correct, are there recommended resistors for this voltage divider? I could not find any surface mount resistors on DigiKey with that rating, and only one thru-hole resistor that met those specifications. It seems odd that this chip requires such a resistor.
Bulk capacitor
3) Section 3.4 (p4) of the Implementation Guide (http://www.ti.com/lit/an/sllu123/sllu123.pdf) recommends the use of bulk capacitors. What are the suggested capacitance values for these? And is it correct that I would want one for each supply rail placed close as possible to the voltage pins on the chip?
4) Would these bulk capacitors be in addition to the Pi filters for the analog supply rails?
Thank you for your help.