Other Parts Discussed in Thread: HD3SS6126EVM, HD3SS6126
Dear sir,
Based on the data sheet for HS3SS6126 the pin number 42, 2, 3, 41 ,38, 37, 36 and 35 are NC (No connection). But in the HD3SS6126EVM there are connection for those pins such a way that its for high speed. I'm confuse with this.
As for the HD3SS6126EVM, there are 2 host (USB 3.0 Micro B) and one input (USB 3.0 Type A).
I do plan to change the 2 host connector(USB 3.0 Micro B) into Type A USB 3.0 connector.
If I change this connector into Type A do I still need to consider pin 42, 2, 3, 41 ,38, 37, 36 and 35 ?