This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Power over STP

Are there any app notes or guidance for sending power over twisted pair when using chips like the DS90UB927 / DS90UB928 ?  Since the twisted pair is capacitively coupled on each end, it seems like it should be possible if done correctly.

Thanks

  • Hi David,

    Check out the EEtimes article that details the Power over FPD-Link concept.

    http://www.eetimes.com/document.asp?doc_id=1279219

    Dac Tran

    SVA APPS

  • Hi Dac Tran
    The article related to POC/PODL is very helpful for designer.
    Hower, I want to have formal application note as the below request.
    Thies because, I am going to design Ti serdes with POC/PODC.
    =========== Below ====================================================================================================
    In case of the 947/948 and 927/928, they need STP cable. Are these possible for supporting PODL? If it can, do you have technical document?
    Another case for Power over Coax, 913/914, If yes for POC (power over Coax), would you give me the related document.
    ========================================================================================================================
    Thanks