Other Parts Discussed in Thread: TUSB2036
I have a hub design that utilizes the TUSB2036 USB Hub and I am trying to verify the design is meeting USB specifications by means of the USBHSET tool set provided by USB.org. I am connected to the Upstream port through a Tektronix USB test fixture which is then connected to a Windows 7 PC running the USBHSET tool set.
With this setup I can enumerate the bus see the TUSB2036 hub and can also initial a few commands (suspend, resume, sleep, wakeup) but when I try to run the Test Packet command, the command fails.
Is the TUSB2036 capable of generating a test packet from a command sent from USBHSET tool?