Other Parts Discussed in Thread: TUSB7340, TPS74401
Hi,
I have a design which uses a TUSB7340. It appears to work correctly (usb devices enumerate, I can talk to them), however it draws a significant amount of power on the 1.1V rail even when idle. The TUSB7340 itself reaches over 90C! So I think something must be wrong.
Furthermore, asserting GRST and PERST has no effect on the power consumption.
The line does not appear to be shorted to ground (when I measure resistance with power off it climbs quickly past 100ohms as caps are charged). The 1.1V line definitely sags (so I don't think it's shorting to 3.3V in some way).
I've attached a photo of my schematic, which is heavily based on the reference schematic.
What might cause this issue?
Thanks! Ben