Other Parts Discussed in Thread: DS90C124, DS90C241
Hi
DS90C124
In my design, you do not use the LOCK pin and ROUT21, ROUT22, ROUT23 of this device.
Since it does not use these terminals, can I get you a open?
Or termination is necessary?
Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Cafain,
Unused outputs may be left open. If you are using a DS90C241 serializer to send the input, then unused inputs are internally pulled-down, thereby ensuring the unused ROUT21-23 outputs are low. The LOCK pin is just a status indicator, and this can be left open if unused.
Thanks,
Michael