Other Parts Discussed in Thread: TUSB9261-Q1, TUSB9261
my chip is TUSB9261-q1 (Automotive grand)
I take the Firmware Binary File (e. g. TUSB926x_FW_v1.04_SATA_NO_POLARITY_SWAP.bin) and load it with the TI Flashburner Tool. In the Advanced Descriptors Editor (Button on top of the window), check "HID Enable", UAS Enable" and "self-powered". Then, Export this data to a bin file. Write this exported bin file (not the original Firmware binary!) to a Flash, using an appropriate programmer.。my board is running ,MISC_LED0#(PWM1)is flashing. but on the demo board SW_HB(GPIO0) is flashing.why they are different? because firmware is different?
1、I didn't plug SSD ,I have got such RS232 results,but my computer can‘t recognize USB device。and Flash Burner can‘t recognize USB device
========================================================
|| TUSB926x Firmware v1.04 [Feb 10 2014 14:39:05] ||
|| Device ID: 0x0000 ||
========================================================
Reset Flag(s): [Power-Up]
[0000000001] Datapath RAM Usage: 80208 / 81920 bytes.
[0000000001] Supported NCQ Depth: 32
[0000000001] U1/U2 Transistions: OFF
[0000000001] USB PHY Suspend: ON
[0000000001] SATA LPM: OFF
[0000000001] Device is Self-powered.
[0000000001] -> usb_hal_init()
[0000000001] USB Core Ver: 0x120a.
[0000000001] USB SSC is OFF.
[0000000051] -> usb_hal_connect()
[0000000051] -> ahci_init()
[0000000051] -> ahci_hba_reset()
[0000000052] USB Reset event occurred.
[0000000052] LTSSM state = (0x7) POLLING.
[0000000306] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000306] -> ahci_port_reset(0)
[0000000361] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000361] -> ahci_port_reset(0)
[0000000416] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000416] -> ahci_port_reset(0)
[0000000471] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000471] -> ahci_port_reset(0)
[0000000526] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000526] -> ahci_port_reset(0)
[0000000581] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000581] -> ahci_port_reset(0)
[0000000636] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000636] -> ahci_port_reset(0)
[0000000691] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000691] -> ahci_port_reset(0)
[0000000746] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000746] -> ahci_port_reset(0)
[0000000801] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000801] -> ahci_port_reset(0)
[0000000856] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000856] -> ahci_port_reset(0)
[0000000911] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000911] -> ahci_port_reset(0)
[0000000966] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000000966] -> ahci_port_reset(0)
[0000001021] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001271] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001271] -> ahci_port_reset(0)
[0000001326] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001326] -> ahci_port_reset(0)
[0000001381] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001381] -> ahci_port_reset(0)
[0000001436] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001436] -> ahci_port_reset(0)
[0000001491] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001491] -> ahci_port_reset(0)
[0000001546] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001546] -> ahci_port_reset(0)
[0000001601] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001601] -> ahci_port_reset(0)
[0000001656] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001656] -> ahci_port_reset(0)
[0000001711] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001711] -> ahci_port_reset(0)
[0000001766] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001766] -> ahci_port_reset(0)
[0000001821] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001821] -> ahci_port_reset(0)
[0000001876] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001876] -> ahci_port_reset(0)
[0000001931] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000001931] -> ahci_port_reset(0)
[0000001986] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000002236] -> ahci_wait_complete() timed out! Rd: 0xfb000128 = 0x00000000, cmplt_val = 0x00000003.
[0000002236] @Error: Timeout waiting for PHY Ready. P0SSTS = 0x00000000, P0SERR = 0x00000000.
[0000002236] Connected to 0 AHCI device(s).
when I plug in a ssd 。But computer(Win XP) can't enumerate the usb 。。。。。。 print like this
========================================================
|| TUSB926x Firmware v1.04 [Feb 10 2014 14:39:05] ||
|| Device ID: 0x0000 ||
========================================================
Reset Flag(s): [Power-Up]
[0000000001] Datapath RAM Usage: 80208 / 81920 bytes.
[0000000001] Supported NCQ Depth: 32
[0000000001] U1/U2 Transistions: OFF
[0000000001] USB PHY Suspend: ON
[0000000001] SATA LPM: OFF
[0000000001] Device is Self-powered.
[0000000001] -> usb_hal_init()
[0000000001] USB Core Ver: 0x120a.
[0000000001] USB SSC is OFF.
[0000000051] -> usb_hal_connect()
[0000000051] -> ahci_init()
[0000000051] -> ahci_hba_reset()
[0000000057] SATA Gen-2 speed negotiated.
[0000002805]
[0000002805] ================================================
[0000002805] IDENTIFY DEVICE INFO
[0000002805] ================================================
[0000002805]
[0000002805] Model: ST320LT012-1DG14C
[0000002805] FW Rev: 0001SDM1
[0000002805] Serial: W3P36A71
[0000002805]
[0000002805] Spec Compliance: ATA-7
[0000002805] Removable Media: No
[0000002805] Rotational Speed = 5400 RPM
[0000002805] UDMA Modes = 0x007f
[0000002805] PIO Modes = 0x0003
[0000002805]
[0000002805] LBA48: Yes
[0000002805] Max LBA = 0x00000000 2542eab0
[0000002805] Write FUA: Yes
[0000002805] World Wide Name = 0x5000c500 7345fbf1
[0000002805]
[0000002805] SATA Speed: Gen3
[0000002805] NCQ Support: Yes
[0000002805] Queue Depth = 31
[0000002805]
[0000002805] Logical Sector Size = 512 bytes
[0000002805] Physical Sector Size = 4096 bytes
[0000002806] Logical Sector Offset = 0
[0000002806]
[0000002806] ================================================
[0000002830] Connected to 1 AHCI device(s).
[0000069435] LTSSM state = (0x5) RX DETECT.
[0000069436] USB Reset event occurred.
[0000069436] -> ahci_reset_lun(0)
[0000069436] LTSSM state = (0x7) POLLING.