Other Parts Discussed in Thread: LMH0387
We're using the LMH0387 interfaced to an Altera Cyclone IV FPGA and are seeing very slow fall times on the SDO and SDO# outputs, approx 10 ns from 90 to 10%. Could this be caused by a ground plane or traces beneath the package?
We missed the section in the data sheet that warns against copper under the package and have a substantial ground area and several SPI interface traces beneath the part. We're in the process of correcting our board design to remove all copper from beneath the package but want to make sure we understand why the fall times are slow before releasing the revised board design.
The data sheet warning only refers to a need for a planar surface on which to mount the package. Are there any electrical risks - of shorted nets, for example - or signal integrity risks that result from having copper under the package?
The FPGA input is configured for LVDS and the SDO signals are DC-coupled to the FPGA. The FPGA pin capacitance is spec'd at ~ 5 pF. The traces between the LMH0387 and FPGA are between 5 and 15 mm long depending on the channel (we have two channels) and are terminated in 100 ohms. Our source is an ASI generator, tested with a variety of cable lengths.
Thanks,
Cor