Other Parts Discussed in Thread: TLK110
I have referenced the following topic, but I have an additional question about the capacitor.
http://e2e.ti.com/support/interface/ethernet/f/903/p/335778/1171952.aspx#1171952
It is recommend to place 10uF and 0.1uF capacitors to pin PFBOUT of TLK110 device. The capacitance between 2 capacitor is difference 100 times. It means that antiresonant frequency will occur at about frequency 15MHz.
Is there any solution to avoid this antiresonant frequency?
Will it be better if I use one 0.1uF capacitor and a Feed Through Capacitor (ex : Murata NFM21PC105B1A3) at the output before connect to PFBIN1, PFBIN2?
Best Regards
Christ