This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VCXO in SD3GDAIII Evaluation Boards

Part Number: ABMM-27

Dear specialist

Could you tell VCXO maker in SD3GDAIII Evaluation Boards since our customer want to refer for their design?

Best regards.

  • Hi Alpha,

    Component X1 is detailed below:

    Manufacturer: Abracon

    Part Number: ABMM-27.000MHZ-B2-T

    Supplier Part Number: 535-9162-1-ND

    It is important to note, however, that though X1 is shown in the User's Guide as a VCXO, the crystal that is on board for the SD3GDAIII Eval Boards is actually just a 27 MHz crystal oscillator (XO), not a VCXO.

    Thanks,

    Michael