Other Parts Discussed in Thread: SN65DSI86
Hello everyone! I am new in this forum.
I am designing a tablet (like ipad).
My mother board is based on a Freescale design
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT
They give me the schematics designs and gerber files.
My main problem is that this board has this video output format:
- Displays – Total five interfaces available. Total raw pixel rate of all interfaces is up to 450 Mpixel/sec, 24bpp. Up to four interfaces may be active in parallel.
-- One Parallel 24-bit display port, up to 225 Mpixels/sec (for example, WUXGA at 60 HZ or dual HD1080 and WXGA at 60 Hz)
-- LVDS serial ports – One port 165 Mpixels/sec or two ports up to 85 MP/sec (for example WUXGA at 60 Hz) each.
-- HDMI 1.4 port.
-- MIPI/DSI two lanes at 1 Gbps.
But my display works with embedded display port. I can not attach you my display datasheet. The model is N133HSE-E21 (innolux)
So I really need a converter from one of these video formats to embedded display port.
I would like to know if you have one chip that convert one of this formats to eDP.
I saw on your website this chip:
http://www.ti.com/product/SN65DSI86/description
I am not a expert in this kind of systems, so I really apreciate if someone with some experience can tell me if this chip or another one could solve my problem.
Kind regards