Other Parts Discussed in Thread: TFP401, DS90C387
Can the TFP401 be used with the DS90C387 for both single LVDS and dual LVDS displays?
Looking at the datasheet I saw that the "DUAL" pin could be pulled high or low to configure the output. If the "DUAL" pin is pulled high then the input signals (single pixel) will be split into odd and even pixel and go to the respective A0-A7 pins. If the "DUAL" pin is pulled low then outputs A4-A7 and clk2 will be disabled and reduce power dissipation.
Will there be a loss of some of the colors since the even pixel outputs would be turned off? Or would it be single pixel in to single pixel out?
Thank you,
Trenton Reed