Other Parts Discussed in Thread: DS110DF111
Hi Team,
Our customer is having trouble using DS110DF111.
The device operates normally at 10GbE, however, CDR is unlocked and the output is muted at 1GbE. I have checked their resistor setting though it seems to be correct.
First, I have asked to set Address 0x3A = 0x00. Then, the symptom had improved a little, but the output still mutes sometimes.
Next, I asked them to try setting the limiting bit for CTLE (Address 0x13 [2] = 1). This setting seems to resolve the problem.
[Q1]
From the results, I am thinking that the device is over compensating. What do you think ?
[Q2]
If it is over compensating, is there any way to lower the gain setting ?
[Q3]
Can we use limiting bit setting in the CTLE setting ?
** I actually have some customer test data which I would like to share. Input eye pattern is open enough but CDR input eye is not clear. I appreciate it if we could discuss about this issue offline.
Best Regards,
Kawai