Other Parts Discussed in Thread: TLK10232
Hi Team,
Please advise me answring to a question bellow.
If LVDS (ANSI-644-A) compliant driver can drive the REFCLK0 or REFCLK1 inputs?
Referring the datasheet (page 98) the “Differential input voltage for REFCLK0/1 must be
from 250 mV to 2000 mV p-p.
In contrast, the LVDS driver output pulse its differential amplitude is 247 to 454 mV p-p.
It is 3mV smaller than REFCLK0/1 input specification.
I wonder if you can change datasheet specification extending the minimum differential
amplitude to 240 mV p-p or much less from 250 mV to accept SNASI-644-A LVDS input?
Mita