Other Parts Discussed in Thread: ISO1540, TCA4311A
Is it possible to use the ISO1540D with a PCA9600 bus buffer (for longer bus range) at both sides? I tried this, also with pull-up's, but it does't work.
What's wrong?
Thanks and best regards!
A.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Andreas,
Side 1 of ISO1540 has its receiver thresholds at ~0.6V. The minimum low threshold on side1 is 0.5V. That is, only if the input signal is below 0.5V will it be detected as a low. It seems the VOL for PCA9600 can be as high as 0.74V. The low level driven by PCA9600 will not be recognized as a low by side 1 of ISO1540. This may be the reason why this scheme is not working for you.
Rgds,
Anant
Hi Anant!
Thanks! It seems you are right. The 2nd side works well with the PCA9600, but not the 1st.
Is there a idea to fix it easy, because the pcb is produced now? I'm afraid, to change the pull-ups isn't the best way...?
Thanks
Hi Andreas,
Even with higher pull up resistors, the VOL from the PCA9600 will remain higher than the IIL of the ISO1540.
I think you need something like the TCA4311A - but unfortunately the pinout is different from the PCA9600.
The other question to ask is if you really need bus extension on both sides? We can discuss by email if you like: anantkamath@ti.com
Rgds,
Anant