This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can we leave the Vdd connection floating on the TPD3E001?

We are using the TPD3E001 for ESD protection of USB signal pairs. 

Now we want to use the part for ESD protection of Gigabit Ethernet pairs.

However the ethernet circuit is a passive PoE injector with only 12 V available as VCC.

Do we need to connect to VCC or can we leave it floating?

I have made a sketch based on the logic block diagram from p. 2 of the datasheet.

Kind regards 

Kasper