Other Parts Discussed in Thread: XIO2221
customer ask me:
1.GUID random write?
2.What organizations can apply for to GUID,have a contact window?
thanks !
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: XIO2221
customer ask me:
1.GUID random write?
2.What organizations can apply for to GUID,have a contact window?
thanks !
sorry!add
3.Use winrom 3.1 write GUID, can be written only once, is there anny way to write many times?it is helpful for factory production
4.Write GUID, must restart the Windows system to find new GUID?
5.Using WINrom load configuration file.Is there any way to write to the configuration file using the command inwindows 8 or DOS.This is helpful to factory automation
6How to quickly check just written to GUID.in wondows 8.do not use winrom tool
thanks!
Hi Will,
I am going to move your question to the Consumer and Computing forum so that it can get the proper support and visibility. They should be able to address you question.
Thanks!
John
Hello,
I am not sure what your application is and why you need to "apply" for a GUID.
The GUID is not mandatory for the 1394 specification, nevertheless, it is recommended for host controllers intended to be used on add-in cards, this is intended to provide vendor-specific information and extended entries to upper level software.
The GUID registers on the XIO2221 can be written via external EEPROM or via PCIe Interface, these Registers are reset only by a PCIe Reset or Global Reset.
We don't have a DOS toll to program the EEPROM.
Regards.