Other Parts Discussed in Thread: TLK106
i am working on a design where i need to connect the MII interface of the AR6400 chipset with the ETH port on a TM4C1294. I was planning on using the TLK10x family of devices to make this connection. The question now is if magnetics are required for a IC to IC connections. These processors will be located on the same PCB. It seems that with no cable length needed, the ETH(RX,TX) from the TLK10x could be connected directly to ETH(TX,RX) of the TM4C1294 in a crossover manner. I have little to no experience with ETH PHY other than using magnetics and a RJ45 connector. Any help would be greatly appreciated.
Thanks
kyle