This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

1394-xio2221 request ~



1.GUID random write?
2.What organizations can apply for to GUIDhave a contact window?E-MAIL address

3.Use winrom 3.1 write GUID, can  be written only once, is there anny way to write many times?it is helpful for factory production

4.Write GUID,  must restart the Windows system to find new GUID?

5.Using WINrom load configuration file.Is there any way to write to the configuration file using the command inwindows 8 or DOS.This is helpful to factory automation

6How to quickly check just written to GUID.in wondows 8.do not use winrom tool

 

thanks!

  • Hello,

    The WinROM was not designed for production lines, if you want to use production tools you can write to one EEPROM and then read the .hex values of that EEPROM so you can then store them into a production programmer or program the EEPROM on the ICT.

     You can set those Register via PCIe using the BIOS, in that way you won’t need an external EEPROM.

    For more information go to the below link

    http://e2e.ti.com/support/interface/digital_interface/f/130/p/377036/1328205.aspx#1328205