This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question on Asynchronous PCI bridge PCI2060



I'm migrating a design from a Pericom PI7C8152B to the PCI2060I bridge for an industrial temperature application.  My system uses the bridge so that the secondary side, which runs from a 33-MHz fixed-frequency oscillator, does not slow down the system when plugged into a 66 MHz primary side bus.  The Pericom chip had a somewhat different clocking scheme and I want to be sure I get it right when I do the re-spin.


In the Pericom part, I needed to use a clock distribution buffer to run the clock from my oscillator to each secondary load and the bridge's S_CLK input pin.  It did not have a separate SEC_ASYNC_CLK input like the PCI2060I.  If I understand it correctly, the PCI2060I should be able to take the oscillator signal (3.3V CMOS) and then all I need to do is configure SEC_ASYNC_RATE high, S_ASYNC_SEL high, and I can use the secondary clocks in the typical fashion of a synchronous bridge, i.e. S_CLKOUT9 looped to S_CLK and other S_CLKOUTx pins to secondary loads.

Is this correct?  Are there any other gotcha's that might prevent the use of this bridge with a fixed 33 MHz secondary clock?  And in this mode, does it matter what I do with the S_M66ENA pin?