Other Parts Discussed in Thread: SN65LVDS3486
Our system uses LVDS to communicate between equipment racks.
The receivers in a turned off rack will blow if the driving rack is still powered.
We are considering a couple of solutions:
1) Use diodes to clamp the receiver inputs to Vcc. This might damage the drivers on the powered up rack because they will drive a heavy load through the forward biased diodes. Most driver data sheets show maximum
2) Use clamp diodes as above and series resistors between the termination resistor and the receiver input. This would limit the current the driver would source through the diodes into the turned off reciever rack. But now performance is degraded by the series resistor/receiver capacitance time constant.
How do we determine the the common mode and normal mode input capacitance of the receiver?
Some TI data sheets specify input capacitance to ground but don't specify differential capacitance. Some data sheets like the SN65LVDS3486 do not specify any input capacitance.
How do we calculate the series resistance so that it is high enough to protect the unpowered reciever while connected to the powered driver?
With this resistance determined, we can calculate the frequency response from the input capacitance if it is specified.
Are there better methods to protect LVDS drivers and recievers in the case I described?
Thank you