Other Parts Discussed in Thread: SN75LVCP601
Hello TI,
We are using the SN75LVCP601 as a SATA repeater, At the input of chip we connected to Mother board using SATA cable and the output of chip was connected to Hard disk. But the hard disk was not detected.
Please go through the above file for reference.
R10: 0 Ohm
R11: Not mounted
We have used all the combinations of DIP switch and also tried by removing all resistors at DIP switch to make DE1,DE2,EQ1,EQ2 as NC.
Please let me know if any thing is going wrong.
Thanks,
Henry