Other Parts Discussed in Thread: TUSB8020B
Hi Team,
Could you please give us your advice to our customer's TUSB8020B situation ?
Our customer's USB host can recognize and work fine with the USB mass storage device and also UAS mass storage device when directly connected to the USB port on the PC.
However, when TUSB8020B USB hub controller is used, USB Host cannot recognize the UAS mass storage device.
They have tested with other two vender's USB hub controller evaluation board. One worked fine but the other had the same situation with TUSB8020B.
If the USB host and the USB device supports UAS, I believe it should be able to communicate correctly. What do you think is the cause to this issue ?
I am currently asking if the USB device has enough Bus voltage as it is BUS powered.
Best Regards,
Kawai